Thanks to Telehealth, the Doctor is… Somewhere
Image Source: mozakim/Shutterstock.com
By Marcel Consée, Mouser Electronics
Published June 25, 2020
Healthcare is deeply personal. Most people associate it with direct contact with doctors, nurses, and medical
equipment. But for some time now, efforts have been made to take contact with medical personnel out of the
equation and make the experience more about equipment. The original idea behind that approach was improving
healthcare in remote locations. But technological advancements, together with economical pressure, have made the
idea popular in many places. Medical crises such as the global Covid-19 pandemic accelerate the adoption of
telehealth methods.
Medical Diagnostics From Body Network To The Cloud - Infographic
E-Health, Telemedicine, Telehealth …
The term virtual healthcare is
used interchangeably with telehealth and
telemedicine. In the U.S., the Health Resources and Services Administration, as well as the Department of Health
and Human Services, defines telemedicine only as remote clinical services, such as diagnosis and monitoring.
At the same time, telehealth includes preventative and curative care delivery, including non-clinical
applications such as administration and provider education. The World Health Organization describes telemedicine
as encompassing all aspects of health care, including preventive care. In Europe, the term eHealth includes
telehealth, electronic medical records, and other components of health information technology.
Whatever it’s called (we will use virtual healthcare here), all forms require excellent communication
infrastructure and ideal broadband connections combined with security software and hardware. Security is a
significant issue when it comes to this kind of data, so encryption is vital for ensuring trust. This type of
information holds a healthcare system together, and electronic health records include critical data such as
medicine dosage, insurance information, and other personal information.
The amount of medical data is growing each year. Before COVID-19 hit, researchers from Stanford University
estimated an annual increase of 48 percent. This figure includes private information regarding patients, their
health status, and insurance providers that circulate in a hospital or doctor's office. Such sensitive
information requires high levels of security for the patients.
That is why most countries have put rules in place to protect electronic personal health information that
health-care providers, health plans, and health-care clearinghouses create, receive, use, or maintain.
Commonly, safeguards are categorized like this:
- Administrative: Assigning security responsibility to an individual and implementing security training.
- Physical: Protect electronic systems and data they hold by restricting access to EPHI and using off-site
backups.
- Technical: Automated processes such as authentication controls and encrypting data during transfer.
Cloud and Edge architectures with adequate security measures can be useful because the exchange of medical data
between clinical facilities, patients, researchers, and medical practitioners requires shifting enormous amounts
of data.
Wearable devices and artificial intelligence
Cloud or edge applications make the use of artificial intelligence (AI) feasible even for smaller practices. Some
specialties in medicine have actually taken up AI techniques over the past few years. The most popular is
radiology, where remote AI platforms routinely process imaging results; from commercial vendors as well as from
research facilities.
The diagnosis itself strongly depends on the relationship between patient and medical practitioner. However, many
diseases can be accurately diagnosed with AI. The most notorious are diabetes and cardiovascular disease (CVD),
which are in the top 10 causes of death worldwide. Because of this high mortality rate, efforts have been made
to integrate various methods in helping get an accurate diagnosis.
Although mobile blood pressure and heart rate monitors, as well as blood oxygen sensors, have been in use for a
long time, the advent of multi-sensor wristbands and sports watches has taken these to a new level. The amount
of data collected by a device such as an Apple Watch is breathtaking. Anyway, not many doctors trust the
1-channel ECG taken by such a gadget, but its alerts can at least advise the wearer to ask for a thorough
medical examination.
A fine example of medical sensor fusion is the MAX86150 Integrated Photoplethysmogram (PPG) and Electrocardiogram
(ECG) Bio-Sensor Module by Maxim Integrated. For development purposes, the manufacturer provides the MAX86150 Evaluation Kit
(Figure 1). ECG, PPG, and simultaneous ECG and PPG can be measured. When monitoring is active,
the module uses IR Proximity Mode to detect the user's fingers, and a red LED will turn on when a finger is near
the module.
Figure 1: The MAX86150 Evaluation Kit provides a proven platform to evaluate
the MAX86150 Integrated Photoplethysmogram (PPG) and Electrocardiogram (ECG) Bio-Sensor Module. (Source:
Mouser Electronics)
Another type of development platform that might be closer to the end product is the MAXREFDES101 Health
Sensor Platform 2.0 (Figure 2), also by Maxim Integrated. The wrist-worn platform
integrates a PPG analog-front-end (AFE) sensor (MAX86141), a biopotential AFE (MAX30001), a human body
temperature sensor (MAX30205) and a microcontroller (MAX32630) together with a power-management IC (MAX20303)
and a 6-axis accelerometer/gyroscope. The complete platform encompasses a watch enclosure and a biometric sensor
hub with an embedded heart-rate algorithm (MAX32664). Algorithm output and raw data can be streamed through
Bluetooth® to an Android app or PC GUI for demonstration, evaluation,
and customized development.
Figure 2: The Maxim MAXREFDES101 Health Sensor Platform 2.0 is a unique
evaluation and development platform in a wrist-worn wearable form factor. (Mouser Electronics)
Conclusion
Virtual healthcare offerings, telehealth, and remote patient monitoring offer several benefits to patients and
physicians. Virtual care has become increasingly popular because of efforts to provide the least-expensive care
in the most effective possible setting. The speed of adoption rises with health crises, but the development of
communication infrastructure has to keep up.
Author Bio
As Technical
Content Specialist, Marcel is the internal contact person for technical questions in Mouser’s EMEA marketing
team. Originally a physicist, he used to work as editor for special-interest magazines in electronics. In real
life, he’s juggling two kids with too many chromosomes, a penchant for electronic gadgets and a fondness of
books and beer. Until now, none has dropped.