Mouser Electronics - Electronic Components Distributor
 
Philippines - Flag Philippines

Please confirm your currency selection:

Pesos
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over ₱2,000 (PHP).

US Dollars
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over $50 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


How Desktop PCB Fabrication Accelerates Hardware Development Mike Parks

PCB milling, conductive ink printing, and laser workflows for rapid prototyping

(Source: diter/stock.adobe.com)

Desktop printed circuit board (PCB) manufacturing is reshaping how hardware is developed and prototyped. The formerly rigid and sequential hardware engineering process is becoming more fluid and integrated. No longer a standalone phase within a larger workflow, fabrication has become part of the in-house design process for many engineers. The ecosystem has matured from a collection of limited tools into a multimodal set of machines capable of producing a PCB layout and a fully soldered prototype in a day.

This blog explores how desktop PCB fabrication has evolved to augment the prototyping workflow. By enabling rapid in-house iteration across milling, printing, and laser workflows, engineers can refine designs quickly before releasing them for production fabrication.

PCB Milling

Mechanical milling systems use precision cutting tools to remove copper from clad stock. Typically, standard materials such as flame retardant 4 (FR-4) are used. Automatic probing routines compensate for surface variation, so cut depth stays consistent, and computer-aided manufacturing (CAM) software works with Gerber files with minimal user intervention. Double-sided boards are routine, and a straightforward design can be milled in under an hour. When the process is well calibrated, debugging results are less likely to be dominated by fabrication artifacts.

The limitations include worn cutting bits and fine-pitch designs (i.e., around 6 mil) that push the limits of what most desktop mills can handle reliably.[1] Milling is inherently subtractive, which constrains material choices to standard laminates. Within those boundaries, though, milling is robust and accessible. However, additive fabrication methods have their own challenges and benefits.

Conductive Ink

Unlike subtractive methods, additive systems deposit conductive material—typically silver-based ink—directly onto a substrate. Many platforms integrate trace printing, drilling, and solder paste dispensing into a single workflow, enabling near-immediate transitions from design to physical output. This makes conductive ink ideal for early-stage work: proof-of-concept designs, education, and flexible substrates where traditional laminates fall short.

Unfortunately, conductive inks have higher resistivity than copper, limiting performance in high-current or high-frequency designs. Many conductive ink systems also face practical limits on resolution and conductivity compared with copper-based subtractive methods. As such, additive printing excels as a rapid exploration tool but is less suited for prototypes that need to closely reflect production intent.

Laser Systems

Laser-based fabrication is one of the more advanced methods for desktop PCB manufacturing. Through photochemical ablation, UV systems can reduce heat-affected zones and lower the risk of charring or delamination compared with traditional thermal processes. Direct copper ablation also reduces or eliminates the need for chemical etching, supporting a cleaner, maskless workflow.

Cost remains the primary barrier, which keeps these systems largely confined to professional labs and well-funded research and development environments. However, continued price declines suggest broader adoption over time. In the meantime, other fabrication methods can be adopted more readily without requiring significant investment.

3D-Printed Circuit Substrates

One of the more practical innovations in desktop PCB fabrication comes from recombining existing tools. Standard fused deposition modeling (FDM) 3D printers can produce functional circuit substrates for certain prototyping tasks. The process begins in an electronic design automation (EDA) tool, with designs transferred to mechanical computer-aided design (CAD) software to convert traces into defined circuit paths. The model is printed, creating a plastic substrate with embedded guides. Copper foil tape is then applied to form the conductors. No copper-clad laminate, etching, or plating is required.

Limitations are significant: wide traces, generous spacing, and typically single-sided designs. Within those constraints, however, the method is effective. 3D-printed PCBs can be produced quickly without expensive tools.[2]

Conclusion

Desktop PCB manufacturing is not defined by a single machine or fabrication method. Milling, conductive ink printing, laser fabrication, and 3D-printed substrates can complement industrial processes. The engineers getting the most value today are those who deploy them selectively, aligning each technique to the specific needs of a given development stage.

Sources

[1] https://support.bantamtools.com/hc/en-us/articles/115003453943-Design-Considerations-for-the-Bantam-Tools-Desktop-PCB-Milling-Machine
[2] https://www.allpcb.com/allelectrohub/mastering-3d-printed-pcbs-a-comprehensive-guide-for-rapid-prototyping



« Back


Michael Parks, P.E. is the co-founder of Green Shoe Garage, a custom electronics design studio and embedded security research firm located in Western Maryland. He produces the Gears of Resistance Podcast to help raise public awareness of technical and scientific matters. Michael is also a licensed Professional Engineer in the state of Maryland and holds a Master’s degree in systems engineering from Johns Hopkins University.


All Authors

Show More Show More
View Blogs by Date

Archives