Mouser Electronics - Electronic Components Distributor
 
Philippines - Flag Philippines

Please confirm your currency selection:

Pesos
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over ₱2,000 (PHP).

US Dollars
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over $50 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: Combining HMI Processing and Real-Time Control on One MCU Mouser Technical Content Staff

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

High-resolution displays are common in everyday life, being integrated into applications ranging from medical and industrial equipment to consumer appliances. As these human-machine interfaces (HMIs) become more sophisticated, they increasingly combine displays, touch controls, voice interaction, and local data processing. While these advancing features give users a better experience, the equipment controlled by these interfaces still needs to perform its primary functions reliably and respond to events in real time.

What is changing amid this evolution is how much of the work a microcontroller unit (MCU) can handle by itself. GHz-class processing, vector acceleration, larger amounts of on-chip memory, and multicore architectures are expanding how much HMI processing, local analytics, and real-time control designers can handle on a single MCU.

Combining these requirements can make embedded systems more complex. Designers need enough processing performance for graphics and data analysis while still maintaining deterministic control of sensors, motors, and other hardware. While previous generations of equipment might have required multiple processors or moving from an MCU to a more powerful application processor, newer, higher-performance MCUs are beginning to shift that boundary between functions.

This week’s New Tech Tuesdays reveals how advanced microcontrollers are blurring the lines with application processors, the architectural benefits of bringing more processing onto a single device, and how the latest MCU designs are transforming modern embedded systems.

Bringing More Processing onto the MCU

Traditionally, MCUs have been optimized for control. Integrating processing, memory, and peripherals has made them a good fit for applications that require predictable responses and direct interaction with hardware. Application processors support more compute-intensive workloads and feature-rich operating systems such as Linux, while MCUs are designed around embedded control and deterministic response.

As embedded HMIs have become more capable, the distinction between these two solutions has become less clear. Modern MCUs can combine GHz-class processing with large amounts of embedded memory in hardware designed to accelerate demanding workloads.

Some of the extra processing power goes toward jobs that once needed additional hardware. For example, audio and sensor data involve repetitive calculations that vector processing can handle efficiently. The same hardware is also useful for machine learning (ML) workloads, such as voice recognition and equipment monitoring.

Multicore devices give designers another way to manage the competing demands. HMI processing might run on one core, while the other responds to sensors or controls a motor. Separating those jobs helps prevent a busy interface or processing task from interfering with tasks that need predictable timing. Meanwhile, keeping more functions on one device can reduce the number of components on the board and how much communication is needed between processors.

Combining workloads this way requires careful allocation of processing time, memory, and peripherals. The question for designers is becoming more about whether the HMI and local processing workload actually require a separate application processor.

The Newest Products for Your Newest Designs®

Renesas RA8M2 microcontrollers demonstrate how this new generation of high-performance MCUs can support greater integration. Built around a 1GHz Arm® Cortex®-M85 core, the RA8M2 provides the processing performance needed for demanding embedded applications while retaining an MCU architecture suited to real-time control.

The Cortex-M85 includes Arm Helium™ technology, providing vector processing capabilities that can accelerate digital signal processing (DSP) and ML workloads, enabling applications such as audio processing, local analytics, and other compute-intensive functions to operate alongside conventional embedded control tasks. Selected RA8M2 devices also include a 250MHz Cortex-M33 core, giving designers another way to partition workloads within the same MCU.

Large integrated memory further supports this approach. With up to 1MB of magnetoresistive random-access memory (MRAM) and 2MB of static random-access memory (SRAM), the RA8M2 can accommodate application code and working data while reducing reliance on external memory. A parallel camera interface and a broad range of communications and peripheral interfaces also allow the MCU to connect directly with many of the devices used by modern embedded systems.

The RA8M2 is targeted at applications where designers need to combine responsive interfaces, connectivity, and local processing while still handling the real-time control expected from an MCU.

Tuesday’s Takeaway

As advanced microcontrollers continue to transform embedded system architecture, high-performance MCUs are changing where designers draw the line between an MCU and an application processor. As MCUs take on more HMI and data-processing work, designers have more options for keeping those functions alongside real-time control. In some systems, that means an MCU may now be enough.



« Back


Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.


All Authors

Show More Show More
View Blogs by Date

Archives