Toshiba TMPM4K4 32-bit Microcontroller, Now at Mouser Electronics, Supports Main and Motor Control for Consumer and Industrial Applications

New Product Press Brief

Connect With Us


Learn more about the TMPM4K4 32-bit microcontroller
Learn more about the TMPM4K4 32-bit microcontroller

July 10, 2025 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Toshiba TMPM4K4 32-bit microcontroller from Toshiba.

The Toshiba TMPM4K4 32-bit microcontroller is based on the high-performing Arm® Cortex®-M4 processor with a floating-point unit (FPU). This microcontroller operates from a 1MHz to 120MHz frequency range and a 2.7V to 5.5V voltage range. The TMPM4K4 microcontroller consists of self-diagnosis functions that support functional safety certification as per IEC 60730 class B and other standards. This microcontroller includes encoder interfaces and programmable motor control functions, which reduce CPU loads during motor control. The TMPM4K4 microcontroller features a 12-bit Analog-to-Digital Converter (ADC), DMA controller (DMAC), CRC calculation circuit (CRC), asynchronous serial communication circuit (UART), and Trigger Selection (TRGSEL) circuit. 

The TMPM4K4 32-bit microcontroller is suitable for applications such as motors, washing machines, refrigerators, and industrial equipment.

To learn more, visit https://www.mouser.com/new/toshiba-semiconductors/toshiba-tmpm4k4-microcontroller/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser is a leading authorized distributor of electronic components and industrial automation products. With more than 6.8 million products from more than 1,200 manufacturer brands, we offer the widest selection of products in stock. Our electronic components business serves the design engineer and buyer communities with New Product Introductions in semiconductors, passive, interconnect and related electronic technologies. Our industrial automation business helps companies design, build and maintain their manufacturing equipment and operations with solutions including the newest sensors, panels, PLCs and motor controls available in stock for immediate shipment.

Mouser provides best-in-class customer service with 28 locations worldwide that offer support in local language, currency and time zone. We ship products daily to more than 650,000 customers in 223 countries/territories from our +1.5 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Toshiba

2026 - Toshiba Electronic Devices & Storage Corporation (TDSC) offers a broad IC and discrete product line-up which includes Power, Small Signal, Optoelectronics, and Logic devices for automotive, multimedia, industrial, telecoms, and networking applications. TDSC develops, manufactures, and supplies innovative storage products including Enterprise and Consumer HDDs.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press inquiries, contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764