SparkFun LilyPad LilyMini ProtoSnap
SparkFun LilyPad LilyMini ProtoSnap is used to learn about creating interactive e-textile circuits before sewing. SparkFun LilyMini ProtoSnap has all its pieces wired together out of the box, like other LilyPad ProtoSnap boards. This allows for testing circuit functions before sewing. At the center of the board is a pre-programmed LilyMini microcontroller connected to a LilyPad Light Sensor, LilyPad Button, and two pairs of LilyPad LEDs.The LilyMini ProtoSnap comes with a pre-loaded code that uses all the LilyPad pieces connected to it. This sample code has three modes, which can be operated by selecting the LilyPad bottom on the bottom-left side of the ProtoSnap.
The built-in RGB LED on the LilyMini changes color to indicate which mode has been selected:
• White: All LEDs on.
• Magenta: LEDs fade in and out in a breathing pattern. When the light sensor is covered, LEDs fade faster.
• Cyan: LEDs off. When the light sensor is covered, LEDs will twinkle.
Kit Contents
- LilyMini (battery included)
- LilyPad light sensor
- LilyPad button
- 4x LilyPad LEDs
Additional Resources
Inilathala: 2019-08-23
| Na-update: 2023-08-04