Now at Mouser: Analog Devices Power by Linear 72V LTC7821 Hybrid Buck Controllers Reduce Solution Size by 50%
May 14, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the Power by Linear™ LTC7821 hybrid step-down synchronous controllers from Analog Devices. The LTC7821 devices are the industry's first to merge a switched capacitor circuit with a synchronous step-down controller, enabling up to a 50 percent reduction in DC/DC converter solution size compared to traditional step-down solutions.
The Analog Devices LTC7821 step-down controllers, available from Mouser Electronics, operate over a wide input voltage range of 10 V to 72 V and can produce an output voltage from 0.9 V to 33.5 V. In a typical 48 V - 12 V, 20 A application, engineers can attain an efficiency of 97 percent with the LTC7821 switching at 500 kHz—three times higher switching frequency than traditional step-down solutions.
The devices' higher switching frequencies enable the use of smaller inductances, leading to faster transient response and smaller solution size, while the soft-switched front end delivers low EMI and reduced MOSFET stress. Boasting extensive protection features, the LTC7821 controllers pre-balance capacitors during startup to prevent the inrush current associated with traditional switched capacitor circuits. The controllers' sense resistor offers overcurrent protection, while system voltage, current and temperature are monitored for faults.
Featuring a proprietary architecture that combines a soft-switching charge pump topology with a synchronous step-down converter, the LTC7821 controllers provide superior electromagnetic interference (EMI) performance and efficiency when compared with traditional switching architectures. Operable over an input voltage range of 10 V to 72 V, the LTC7821 controllers can generate an output voltage range of 0.9 V to 33.5 V with ±1 percent accuracy.
The LTC7821 controllers' powerful 1-Ohm N-channel MOSFET gate drivers maximize efficiency and can drive multiple MOSFETs in parallel for higher power applications. With its current mode control architecture, multiple LTC7821 devices can be operated in a parallel, multiphase configuration with excellent current sharing to enable much higher power applications. The LTC7821 step-down controllers are suitable for next-generation non-isolated intermediate bus applications in datacom and telecom. The controllers are also ideal for high current distributed power systems and emerging 48 V automotive systems.
To learn more, visit www.mouser.com/adi-ltc7821-hybrid-controllers.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Analog Devices Inc.
Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com