Robust Diodes Incorporated New ZXGD3009 Gate Drivers Available from Mouser
January 7, 2015 - Mouser Electronics, Inc. is now stocking the new ZXGD3009 High Speed Non-Inverting Gate Drivers from Diodes Incorporated. These rugged gate drivers boast a near-zero quiescent supply current and can transfer up to 1 Amp peak source/sink current into the gate for effective charging and discharging. They are designed to withstand harsh environments, ESD spikes, and latch-up conditions.
The new Diodes Incorporated ZXGD3009 High Speed Non-Inverting Gate Drivers, available from Mouser Electronics, are robust gate drivers designed for the rapid switching of MOSFETs under harsh conditions. These gate drivers can withstand electrostatic discharge shocks of up to 4,000V (HBM) without harming the device. A wide supply voltage allows for up to 40V drive voltage. These drivers can typically drive 500mA into the low gate impedance with just a 10mA input, allowing direct drive from an output pin from most microcontrollers. This reduces bill of materials cost by eliminating the need for an intermediate buffer.
These new gate drivers require a minimum of external components, with a pinout configuration optimized for simplifying printed circuit board layout, along with the added advantage of reducing parasitic trace inductances. The turn-on and turn-off behavior of the controlled MOSFET, including ramp-up and ramp-down times, can be modified to suit individual applications. This allows fine-tuning the developer's circuit so that electromagnetic interference and cross-conduction problems can be reduced or eliminated. The emitter-follower is designed to tolerate, and be immune to, potential latch‑up or shoot‑through situations.
The datasheet contains a useful application diagram. Target applications for the ZXGD3009 Gate Driver include power supplies, DC to DC converters, audio amplifier output stages, and motor control.
To learn more, visit: http://www.mouser.com/new/Diodes-Inc/diodes-inc-zxgd3009-drivers/ .
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Diodes Incorporated
Diodes Incorporated is a leading global supplier of high-quality application specific standard products within the broad discrete and analog semiconductor markets. Diodes products include diodes, rectifiers, transistors, MOSFETs, protection devices, function-specific arrays, amplifiers and comparators, Hall-effect sensors and temperature sensors, and power management devices including LED drivers, DC-DC switching regulators, linear voltage regulators and voltage reference, as well as special function devices including USB power switch, load switch, voltage supervisor and motor controllers.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Corporate Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com