Mouser Powers Up with the Maxim Integrated MAX77818 Switching Mode Battery Charger for Handheld Devices
August 19, 2015 - Mouser Electronics, Inc. is now stocking the MAX77818 Switching Mode Charger from Maxim Integrated. One of the industry's smallest and fastest battery charging programmable switching mode chargers, this power management integrated circuit (PCIM) utilizes several charging states to safely and quickly charge a wide range of one-cell lithium ion (Li+) or lithium polymer (Li-poly) battery sizes and system loads. Based on Maxim's proprietary ModelGauge™ (mg5) fuel gauge technology, the MAX77818 features a dual-input, Smart Power Path 3.0A switch mode charger with frame ground (FG), reverse boost capability, and adapter input protection that withstands up to 16VDC.
The Maxim Integrated MAX77818 Switching Mode Charger, available from Mouser Electronics, features a high, 4.0MHz switching frequency on the DC-DC converter, which is ideally-suited for portable devices. This dual-input, switch-mode DC-DC converter includes integrated, low-loss switches, and allows the use of small components while eliminating excessive heat generation. The chip supports both buck and boost modes. Battery charge current on the MAX77818 is programmable from 0A to 3.0A, and the charger's two inputs accept adapter/USB (CHIN) and/or wireless type inputs (WCIN). The wireless input can simultaneously charge the battery while powering up USB-OTG type accessories, while the USB-OTG output provides true-load disconnect and is protected by an adjustable output current limit.
Using Maxim's Smart Power Selector architecture, the MAX77818 supplies up to 3.0A continuous (4A peak) buck mode current. A supplemental mode provides additional current from the battery to the system up to 4.5ARMS. Power not used for the system goes to charging the battery, and all power switches for charging and switching the system load between battery and adapter power are included on chip - no external MOSFETs are required. The battery charger includes Smart Power Path and I2C adjustable settings to accommodate a wide range of battery sizes and system loads, and several safety features ensure reliable charging. The MAX77818 provides accurate battery fuel gauging without calibration and operates with extremely low battery current due to its ModelGauge (mg5) battery fuel gauge.
Maxim's Integrated MAX77818 Switching Mode Charger is available now through Mouser Electronics in a 72-bump, 3.867 mm × 3.608 mm WLP package, and is ideally suited for a variety of portable applications including smartphones, tablet computers, and other handheld devices.
To learn more, visit http://www.mouser.com/new/maximic/maxim-max77818-charger/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Maxim Integrated
Maxim is the leader in analog integration. From mobile to industrial solutions, Maxim is making analog smaller, smarter and more energy efficient.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com