Terabee Air Quality SB5 Monitor
Terabee Air Quality SB5 Monitor measures CO2, particulate matter (PM 1, 2.5, 4, 10), and total volatile organic compounds (TVOC) index. Additionally, this monitor measures air temperature and relative humidity, ensuring the five most in-demand ambient metrics are measured. The measured data is directly integrated into the system via Wi-Fi® and HTTP/HTTPS data protocol. Terabee Air Quality SB5 Monitor has multifunction visual signals, including network status, air quality, and operation mode.Features
- Carbon dioxide concentration (CO2)
- Total Particulate Matter (PM 1, 2.5, 4, 10)
- Total Volatile Organic Compounds (TVOC) Index
- Air temperature (°C and °F)
- Relative humidity
- Setup via Wi-Fi Access Point
- Multifunction visual signal of network quality, air quality, and operation mode
- Communication of air quality measurements through HTTP/HTTPS protocol via Wi-Fi
- Remote firmware update by Terabee
Applications
WHY USE THE INDOOR AIR QUALITY SENSOR FROM TERABEE?
With the Terabee Air Quality SB5, users can measure five metrics simultaneously, gathering data on CO2 and PM levels and the TVOC Index, temperature, and relative humidity. Data is available for direct integration into systems without the need for a subscription model, which means users can use it more quickly, and without the cost of subscription fees.
The simple and neat design, with the provision of a visual indicator of the air quality in an indoor room or space, means that users see the air quality immediately.
State-of-the-art Swiss-made Sensirion sensors feed all the air measurements into the results.
IMPROVE WELL-BEING AND WORK EFFICIENCY IN OFFICES
Do users know the air quality measurement in their building or office space? Labor and workplace codes recommend that air in closed work areas be renewed to maintain healthy air quality and avoid excessive temperature rises.
Terabee Air Quality SB5 allows users to collect data on the environment and air pollutants to adjust the ventilation or air conditioning system according to defined air quality metric thresholds.
MAINTAIN AIR QUALITY AND COMFORT IN PUBLIC FACILITIES
Studies by the World Health Organization show that optimizing air quality enhances the productivity and well-being of building occupants and reduces the transmission of allergies and illnesses.
Be sure that users have the indoor air quality tools needed to be able to ensure that staff and visitors are comfortable and have the best possible air to breathe.
With its real-time indicators of CO2, PM 1, 2.5, 4, and 10, TVOC Index, temperature, and relative humidity, the Terabee Air Quality SB5 gives users confidence that heating, ventilation, and air conditioning systems are working optimally and allows intervention when they are not.
OPTIMIZE THE ENERGY PERFORMANCE OF A BUILDING
With accurate air quality metrics, users can make energy savings. Here’s how. Analyze the correlation between occupancy and air quality metrics of a building. When users have accurate, up-to-date indoor air quality data, they can make informed decisions about how to maximize the quality of the air with the best use of the ventilation system.
Optimize the programming logic of the HVAC system. Use the data from the five metrics that the SB5 provides to make the most of energy efficiencies with the ventilation programming to use it when needed.
EASY TO DEPLOY IN ANY PUBLIC FACILITIES OR SMART BUILDINGS
As manager of a public facility or building, they should know the air quality to provide the best possible environment for building users. The Terabee Air Quality SB5 is easy-to-install and maintain, which means it’s ideal to use in public facilities such as offices, schools, libraries, and information centers.
For smart building managers, having accurate air quality data at their fingertips means making informed decisions to improve indoor air quality in the building when the metrics go below the accepted threshold.
A full installation guide is provided with the product.
EASY-TO-READ LED STATUS
A Green > Orange > Red LED indicates the air quality, while a full suite of measurements is sent directly via WiFi through HTTP/HTTPS data protocol to the platform of your choice. With its visible LED air quality indicator, users can be assured that they are working with suitable air quality. Should the air quality degrade, ventilation can be increased so you remain in control of the quality of air.
Dimensions
Kit Contents
- Quick Start Guide
- 1 AC/DC USB-C power adapter with changeable plugs from the US, UK, and EU
- 1 x Terabee Air Quality SB5
- 1 x 2-meter USB-C cable
- Concrete and plaster wall screws and table mount accessories